vl Control Effort
| Index.Sub | 6044.0H |
| Data Type | Integer16 |
| Access | Read Only |
| PDO Mappable | TX_PDO (1) |
| Unit | User-defined velocity unit |
|
Range |
Integer16 |
| Default Value | No |
| Store Supported | No |
| Description |
This object is used for ‘Velocity mode (vl)’ and is the velocity at the motor spindle or load (without closed loop control this value reads the vl Velocity Demand. Positive values shall indicate forward direction and negative values shall indicate backward direction. The User-defined velocity unit is converted to the revolution per minute (rpm) with vl Dimension Factor (numerator): Velocity [user-defined units] x vl Dimension Factor (numerator) = Velocity [rpm] The ‘device internal velocity unit’ is ‘rpm’ [revs/min]. |
|
Notes |
(1)Available with firmware V00r74 or superior. |